The maximum voltage and current power points can be found in the Operating Manual. See http://literature.cdn.keysight.com/litweb/pdf/N8900-90901.pdf#page=18.
The easiest way to determine if a voltage combination exceeds the power limit of your supply is to multiply the desired output voltage by the desired output current.
If the result is greater than the maximum power rating of your power supply (either 5 kW, 10 kW, or 15 kW) then the voltage/current combination cannot be generated by your power supply model.
Applies to: N8920A, N8921A, N8923A, N8924A, N8925A, N8926A, N8928A, N8929A, N8930A, N8931A, N8932A, N8934A, N8935A, N8937A, N8937APV, N8940A, N8941A, N8943A, N8944A, N8945A, N8946A, N8948A, N8949A, N8950A, N8951A, N8952A, N8954A, N8955A, N8957A, N8957APV
Visit our Power Products Forum for additional topics and discussions. Read technical postings on our Power Blog – Watt’s Up? |